In the Physical
Channel node, select a PDCCH channel, then click the
button in the Transmission
Configuration cell to open the PDCCH Transmission Configuration dialog
box. Click the Column Preset button
to access a
drop-down
list
that enables you to set the parameters for all PDCCH transmissions to
the same value.
Choice: On | Off
Default: Off
Check (On) or clear (Off) to set the channel state.
Use the Data Source Selection dialog box to select , , or to use for the data.
Use the drop-down list to select a control channel element (CCE) aggregation level of 1, 2, 4, or 8.
The choices available for control channel element (CCE) offset are determined by the CCE aggregation level as follows:
|
CCE Aggregation Level |
CCE Offset choices |
|---|---|
|
1 |
0 | 1 | 2 |... N_PDCCHmax -1 |
|
2 |
0 | 2 | 4 |... N_PDCCHmax -1 |
|
4 |
0 | 4 | 8 |... N_PDCCHmax -1 |
|
8 |
0 | 8 | 16 |... N_PDCCHmax -1 |